Notice: Function _load_textdomain_just_in_time was called incorrectly. Translation loading for the business-units-for-igus domain was triggered too early. This is usually an indicator for some code in the plugin or theme running too early. Translations should be loaded at the init action or later. Please see Debugging in WordPress for more information. (This message was added in version 6.7.0.) in /var/www/html/wp-includes/functions.php on line 6121 Warning: Cannot modify header information - headers already sent by (output started at /var/www/html/wp-includes/functions.php:6121) in /var/www/html/wp-content/themes/business-units-for-igus/functions.php on line 386 Bearing – 易格斯新闻技术资讯

Category:

Bearing

Seat height adjustment – permanently quiet thanks to innovative plain bearing designs

Ethen Liang | June 7, 2022

The innovative assembly concepts of igus plain bearings are particularly popular for hinge connections in, amongst other things the seat height adjustment. The igus clip bearings are easy to handle and increase efficiency. The flange processes and recalibration steps common to metallic plain bearings are eliminated. Further advantages are the weight (up to 5x lighter) and parts price reduction (up to 40%) compared to the metal version.

Read more...

Are plain bearings with thick walls advantageous in heavy-duty applications?

Yvan Cao | March 1, 2022

Metallic plain bearings with relatively thick walls (conforming to DIN 1850, for instance) are used in many heavy-duty applications in agricultural engineering and construction machinery…

Read more...

sustainable automotive

Sustainable vehicle design with iglidur® plain bearings

Ethen Liang | January 19, 2022

Current trends such as zero-emission vehicles or CO2-neutral production demonstrate the growing importance of sustainability in the automotive industry….

Read more...

ticket machine

Why your ticket machine ball bearings should be from igus®

Daniel Chen | September 24, 2021

Ball bearings in ticket machines where requirements for installed components are stringent. igus polymer ball bearings are expanding their advantage over metal ball bearings in this segment. They are not only maintenance-free and lubrication-free – they also ensure that the application environment is free of contamination. Searching for contamination…

Read more...

滚珠轴承的替换

Ball bearing alternative made of polymer: igus® convinces

Daniel Chen | September 17, 2021

Many plant operators know the problem: when installing metal ball bearings, lubrication is essential. This procedure has to be repeated at regular maintenance intervals and that not only swallows up money, but also a lot of time. As a ball bearing alternative, xiros is particularly suitable…

Read more...

iglidur聚合物滚珠

Polymer coating – the way to protect parts from wear and tear

John Ji | September 15, 2021

Surface coatings have long since established themselves in all areas of everyday life. From frying pans to bicycle frames, the range of different coating materials and their properties is huge. A more recent phenomenon is the so-called tribological polymer coating. These are plastic-based coatings that have been additionally improved tribologically – i.e. for use as a friction-optimised surface. Thus, metallic surfaces not only protect against corrosion or scratching, but also against abrasion by other friction partners. The main advantage…

Read more...

汽车内饰

Why are polymer ball bearings so interesting for vehicle interiors?

Ethen Liang | August 19, 2021

Developing the interiors of cars is a big challenge for designers and engineers. Within just a few seconds, it creates a first gut feeling. Even before we sit down on the car seat, we reach for the steering wheel. Immediately afterwards, we examine the arm rest and feel the buttons for adjusting the windows…

Read more...

易格斯自润滑免维护轴承

When should I change my ball bearing?

Daniel Chen | August 13, 2021

Change the ball bearing? This should be done, when …

the bearing clearance caused by wear has reached an unacceptable level, for example, when the shaft “sags”.
the cage is worn and in danger of falling out.

Read more...

Reduce costs in vending machine construction with reliable components

Ahren Xia | July 20, 2021

Whether the snack dispenser in an office, the reverse vending machine in a shop or an ATM on the street, they all have to

Read more...

聚合物涂层

Polymer coating – the way to protect parts from wear and tear

John Ji | July 16, 2021

Surface coatings have long since established themselves in all areas of everyday life. From frying pans to bicycle frames, the range of different coating materials and their properties is huge. A more recent phenomenon is the so-called tribological polymer coating…

Read more...