Bearing
Ball bearings have become indispensable in mechanical engineering. There are various ball bearing designs for which mass and technical composition of the components depend on the specifications of the industrial application. The following list shows the most frequently used ball bearings and where they are used…
We have often dealt with this problem. Simple plain bearings are used in most applications. As these are usually seated with a positive fit and fixed in a housing hole, it is almost impossible for them to fall out or break…
When do I use a particular ball bearing? – Metal, plastic, ceramic.Choosing the right material for ball bearings is not always easy. A short summary, when I use a particular ball bearing…
The safety of food and drink is crucial to the well-being and health of people around the world. The cleaning and disinfection of food and beverage machines is therefore extremely important…
This is an online seminar organized by igus.inc. The speakers made a thorough study on noise, noise sources, noise reduction solvement, and related applications such as pedals, steering gear, seats and hinges. The logic is clear and the reference cases are very valuable. The duration is about 24 minutes. Welcome to click and watch!
Vending machines are becoming increasingly popular not only among farmers. It’s been a long time since they only served packaged drinks and snacks. Whoever loves to get hot pizza, fried chips or even milk from the farmer, he or she can get it from a vending machine around the corner.All this around the clock without employees..
14 client companies, 46 representatives.In addition to that we have also our own colleagues.As the first online customer-oriented conference, the online seminar size actually exceeded our expectations.
Maintenance is a central point when operating machines. On the one hand, this ensures operational safety. On the other hand, maintenance is associated with expenditure. This expenditure is divided up as follows: The machine is at a standstill during maintenance. Depending on the machine, this is expensive. A construction machine cannot be rented. And problematic depending […]
During extrusion polymers are continuously melted and extracted through the extrusion die and brought into shape. In this way, bar stock such as filaments, profiles, plates or films emerge; the so-called extrudate…
Case study There is little doubt that a shaft damaged by corrosion has a negative effect on the bearing point. It is especially obvious that the shaft is damaged when the corrosion is easy to see – and the surface apparently has already disappeared. But appearances can be deceiving.And that leads to a search for […]