Bearing
Large bearing diameters tailor-made at an off-the-shelf price! The largest selection of different dimensions is offered by “the generalist” iglidur G. The smallest bearing has an inner diameter of 3mm (smaller inner diameters are available for other iglidur materials). The largest inner diameter of an igus catalogue part is 195mm. Part No.: GFM-195205240-65 (Outer diameter 205mm, flange […]
Almost all cars are now equipped with differentials. What is its function?The differential of a car is the system that regulates how fast the tires rotate individually and helps you turn left and right. So differentials solve the cornering problem, but they come with a huge disadvantage for off-road driving. Supose that a right wheel […]
In a motion structure, a shaft and a bearing constitute an operating unit. In this sense, wear and friction values need to be evaluated from an overall perspective. To optimize lives, materials of the shaft and the bearing need to be perfectly coordinated, which is a main challenge for bearing manufacturers today. For the shaft, […]
In order for an assembly or component to be allowed for use in a modern rail vehicle in Europe, the components must be tested and evaluated according to EN45545. This is a very time-consuming, bureaucratic process. The exposed surface, the weight of the component, and many other points must be considered for selection. So where […]
Widespread in the animal kingdom, for people an option. The skeleton on the outside of arthropods provides stability in the same way as the endoskeletons of mammals. Why not combine the advantages of the two systems with each other? An endoskeleton (inside the body) is strong but, having numerous joints, is nevertheless very flexible. It […]
When refering to modified vehicles, we are now easily thinking about a foldable steps of SUV,especially those with high chassis. In order to help passengers to easily get on and off, installing a set of steps is almost a must. There are 2 types of step for your option:fixed or foldable. Nowadays more and more […]
igus experts will show how motion plastics can reduce costs and improve technical performance in the automotive area.
… Are you familiar with these air diffusers that bring cool airflow into rooms when outside temperatures are too high? Did you know that they sometimes move in order to distribute and regulate said airflow? In the case of simple air diffusers for air conditioning units, the risk to mankind is limited. But…
Since food and beverages are sensitive products, production and processing must also be precisely tailored to them. This applies in particular to direct food contact.For this reason, there are igus materials that have been specifically developed for the requirements of the food and beverage industry.
Grease or lubricating oil is essential for installing metal ball bearings. With xiros polymer ball bearings you can enjoy 100% lubrication-free ball bearings made of plastic. No grease No oil No residues on hands or machines!