Bearing
The modern car interior has many different knobs, dials and switches. Whether it is the adjustment of the window, air conditioning or sound level – we are increasingly resorting to the cleverly placed rotary adjusters in the interior. All these controls are directly related to the quality perception of the vehicle and can influence a […]
Manufacturer of filling systems, miromatic, uses the igus modular construction kit Machines from miromatic fill containers with foodstuffs such as yoghurt fully automatically. The requirements regarding the hygiene and availability of the machines in such cases are high. The igus plain bearings made of high-performance plastics with incorporated lubricant prove their worth under these conditions.In […]
Why auto customers trust in the DryLin linear guide products?With the advantages of free of lubrication, lighter than metal materials, quiet operation and fast delivery, we have attracted a lot of customers in the auto industry for many years, in this article you will find the answers of this question. What is DryLin? DryLin® is […]
The Xiros self-lubricating plastic ball bearing is adopted for the shutter mechanism of the active air intake grille, which could perfectly meet the requirements of the customers: it features minimum friction coefficient, dirt resistance, resistance to high temperature and low temperature and light weight. For vertical shutter, we also provide iglidur J sliding bearing for […]
Just recently I stumbled on this blog post, which promised to finally put an end to the mystery that seems to be iglidur®. What is iglidur? And why are customers willing to spend no less than a fortune on bearings made from this material? To make this clear right away: I have no intention to […]
In the bicycle industry, innovative solutions are not only focused on design, but also on the choice of materials. For example, for the frame there are many solutions made of aluminium or glass fibre reinforced material. Component manufacturers are also working flat out on the use of alternative materials. Be it saddle post, suspension, pedals […]
On June 27, 2020, Shanghai officially announced the launch of Didi’s self-driving service online, which signify that driverless technology and applications have basically matured. Without a driver, or the driver adjusts to automatic driving mode, the internal space of a car can be transformed into entertainment room,or games, rest , meeting room. Passengers can adjust […]
iglidur® bearings are press-fit bearings for bores with a H7 standard bore. On the one hand, this press-fitting fixates the bearings in the housing and on the other, the inner diameter of the bearings is formed by that and finally creates the proper inner tolerance. If you measure the loose bearings as delivered, the inner- […]
Thanks to our modern injection molding production process, the desired iglidur® plain bearing can be manufactured in almost any geometry, for example as a flexible iglidur® clip bearing or flanging sleeve especially for quick assembly in sheet metal solutions. This design is used in hinges and seats in automobiles, and igus is constantly optimizing and […]
The automotive thermostat is a valve that controls the flow of engine coolant, whose temperature can neither be too high nor too low. The thermostat can automatically adjust the amount of water entering the radiator according to the temperature of the coolant to keep it at the optimal working temperature, which is important for the […]