Notice: Function _load_textdomain_just_in_time was called incorrectly. Translation loading for the business-units-for-igus
domain was triggered too early. This is usually an indicator for some code in the plugin or theme running too early. Translations should be loaded at the init
action or later. Please see Debugging in WordPress for more information. (This message was added in version 6.7.0.) in /var/www/html/wp-includes/functions.php on line 6121
Warning: Cannot modify header information - headers already sent by (output started at /var/www/html/wp-includes/functions.php:6121) in /var/www/html/wp-content/themes/business-units-for-igus/functions.php on line 386
topteaser
required for Theme
Metallic plain bearings with relatively thick walls (conforming to DIN 1850, for instance) are used in many heavy-duty applications in agricultural engineering and construction machinery…
Ball bearings in ticket machines where requirements for installed components are stringent. igus polymer ball bearings are expanding their advantage over metal ball bearings in this segment. They are not only maintenance-free and lubrication-free – they also ensure that the application environment is free of contamination. Searching for contamination…
Developing the interiors of cars is a big challenge for designers and engineers. Within just a few seconds, it creates a first gut feeling. Even before we sit down on the car seat, we reach for the steering wheel. Immediately afterwards, we examine the arm rest and feel the buttons for adjusting the windows…
Sintered bushings or plain bearings made of sintered bronze are used in many bearing applications. They are comparatively cheap to procure, available in many dimensions and are sold as “self-lubricating” or “maintenance-free”…
The weather is getting nicer and the sun is shining longer and more intensively. It is not only us humans who replenish energy, photovoltaic systems literally do so. These are exposed to enormous weathering effects all year round, and the surfaces reflect this especially when the sun shines…
Ball bearings cover a wide range of different shapes. Whether deep groove ball bearings, ball bearings with flange, for example, or self-aligning ball bearings: standard catalogues list these in various materials, designs and dimensions. But what about customised solutions? Customised ball bearings are no stranger to igus…
Most linear bearings, whether with metallic balls, rolling elements, coating or bonded elements, cannot be reused because of their design. For the user this usually means ordering new linear housings. This results in costs for re-procurement and delivery times. Proper disposal is also an additional challenge. Many bearings must be disposed of in hazardous waste due to the lubricants used.Not so with igus…
How does the production of lead screws actually work? What are the processes available and what is the difference between the thread rolling and thread whirling manufacturing processes?
To find out, we should first compare the two manufacturing methods of thread rolling and thread whirling…
iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, round bars, or hollow rods made of various high-performance iglidur polymers & in a wide range of sizes and dimensions.
Many different shaft materials are used in the packaging, food and beverage industries. If a cost-effective solution is required, steel shafts are of interest. If light weight is important, aluminium shafts are used. If the application takes place in a humid environment or aggressive cleaning with chemicals, the corrosion resistance of the shaft is important. Stainless steel is a good choice here…