Notice: Function _load_textdomain_just_in_time was called incorrectly. Translation loading for the business-units-for-igus
domain was triggered too early. This is usually an indicator for some code in the plugin or theme running too early. Translations should be loaded at the init
action or later. Please see Debugging in WordPress for more information. (This message was added in version 6.7.0.) in /var/www/html/wp-includes/functions.php on line 6121
Warning: Cannot modify header information - headers already sent by (output started at /var/www/html/wp-includes/functions.php:6121) in /var/www/html/wp-content/themes/business-units-for-igus/functions.php on line 386
Packaging industry
包装行业
iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, round bars, or hollow rods made of various high-performance iglidur polymers & in a wide range of sizes and dimensions.
Many different shaft materials are used in the packaging, food and beverage industries. If a cost-effective solution is required, steel shafts are of interest. If light weight is important, aluminium shafts are used. If the application takes place in a humid environment or aggressive cleaning with chemicals, the corrosion resistance of the shaft is important. Stainless steel is a good choice here…
There are many different possibilities to synchronise several adjustments in one system. But which is the right one for me and my application? Often not easy to answer. But what if it should be simple and uncomplicated?
When the corona pandemic (COVID-19) broke out, many companies volunteered to manufacture medical products such as masks, gowns, ventilators and face shields. In addition to the FDA-compliant materials used for the actual masks, gowns, ventilators and face shields, the tools and machinery used to manufacture these products must also meet FDA compliance standards…
The concern is often optimisation of component or system service life. In the packaging and beverage industries, machines operate at especially high frequencies, and component service life plays an important role. But it can be just as important to extend the product service life or life cycle. ..
igubal spherical bearings are self-aligning bearing elements manufactured completely from polymer and are therefore very lightweight. They are perfect for use in weighing systems…
igus has many different linear guides in its product range. For example, drylin W offers a large modular system. drylin N is the first choice for extremely low-profile installation heights. drylin T is identical in construction to the usual recirculating ball bearing guides. A representative of the shaft guides is drylin R. Since some machine […]
Wherever food or beverages are processed, filled or packed, contamination can occur. If it is salt or sugar, it is important to take a close look at the abrasive (rubbing/grinding) wear. In this way it can be determined what influence this has on the plain bearing or linear guide…
To maximise flexibility, machines and equipment in the packaging, food and beverage industries must be capable of implementing precise format adjustments. This equipment might be filling or labelling machines for bottles or cans, but can also be entry lanes in material handling…
We have often dealt with this problem. Simple plain bearings are used in most applications. As these are usually seated with a positive fit and fixed in a housing hole, it is almost impossible for them to fall out or break…