topteaser
required for Theme
This is an online seminar organized by igus.inc. The speakers made a thorough study on noise, noise sources, noise reduction solvement, and related applications such as pedals, steering gear, seats and hinges. The logic is clear and the reference cases are very valuable. The duration is about 24 minutes. Welcome to click and watch!
14 client companies, 46 representatives.In addition to that we have also our own colleagues.As the first online customer-oriented conference, the online seminar size actually exceeded our expectations.
During extrusion polymers are continuously melted and extracted through the extrusion die and brought into shape. In this way, bar stock such as filaments, profiles, plates or films emerge; the so-called extrudate…
Case study There is little doubt that a shaft damaged by corrosion has a negative effect on the bearing point. It is especially obvious that the shaft is damaged when the corrosion is easy to see – and the surface apparently has already disappeared. But appearances can be deceiving.And that leads to a search for […]
Everyone knows that the agricultural and construction machinery sector require lots of care. Dirt, moisture, corrosion, the complete package. Whether a combine harvester, tractor, concrete mixer, plough or mobile crane – here everything is in the same boat. Metallic plain bearings are always lubricated – at least they should be if they are to function. […]
Cat-HTR technology developed by a German scientist regains resources from plastic waste in 20 minutes
There must be an answer to this question. After all, there are a limited number of “best Italian restaurants”, “best frozen pizzas” and “best TV series”. And we haven’t even got to narrowing it down. The best Italian restaurant in Bonn? Or in the whole world? The question of the best plain bearing for farm […]
Almost all cars are now equipped with differentials. What is its function?The differential of a car is the system that regulates how fast the tires rotate individually and helps you turn left and right. So differentials solve the cornering problem, but they come with a huge disadvantage for off-road driving. Supose that a right wheel […]
In order for an assembly or component to be allowed for use in a modern rail vehicle in Europe, the components must be tested and evaluated according to EN45545. This is a very time-consuming, bureaucratic process. The exposed surface, the weight of the component, and many other points must be considered for selection. So where […]
igus extends ISO Class 1 energy chain series with single chamber solution and e-skin flat with support chain for more unsupported lengths