Category:

Plain Bearings

防火

The right plain bearings for air diffusers & sleepless nights in Shanghai

John Ji | September 18, 2020

… Are you familiar with these air diffusers that bring cool airflow into rooms when outside temperatures are too high? Did you know that they sometimes move in order to distribute and regulate said airflow? In the case of simple air diffusers for air conditioning units, the risk to mankind is limited. But…

Read more...

食品认证

Certifications for the food and beverage industry

Ahren Xia | September 18, 2020

Since food and beverages are sensitive products, production and processing must also be precisely tailored to them. This applies in particular to direct food contact.For this reason, there are igus materials that have been specifically developed for the requirements of the food and beverage industry.

Read more...

无润滑球轴承

Why lubrication-free is a better option for your ball bearing

Daniel Chen | September 18, 2020

Grease or lubricating oil is essential for installing metal ball bearings. With xiros polymer ball bearings you can enjoy 100% lubrication-free ball bearings made of plastic. No grease No oil No residues on hands or machines!

Read more...

miromatic公司专注于生产水果酸奶搅拌和桶装食品灌装设备,是这一领域的欧洲企业领导者。

Hygienic design with plastic plain bearings

Ahren Xia | September 16, 2020

Manufacturer of filling systems, miromatic, uses the igus modular construction kit Machines from miromatic fill containers with foodstuffs such as yoghurt fully automatically. The requirements regarding the hygiene and availability of the machines in such cases are high. The igus plain bearings made of high-performance plastics with incorporated lubricant prove their worth under these conditions.In […]

Read more...

主动进气格栅

Active Air Intake Grille

Lynna Liu (刘银) | August 31, 2020

The Xiros self-lubricating plastic ball bearing is adopted for the shutter mechanism of the active air intake grille, which could perfectly meet the requirements of the customers: it features minimum friction coefficient, dirt resistance, resistance to high temperature and low temperature and light weight. For vertical shutter, we also provide iglidur J sliding bearing for […]

Read more...

Advantages of polymer bearings in the bicycle

John Ji | August 10, 2020

In the bicycle industry, innovative solutions are not only focused on design, but also on the choice of materials. For example, for the frame there are many solutions made of aluminium or glass fibre reinforced material. Component manufacturers are also working flat out on the use of alternative materials. Be it saddle post, suspension, pedals […]

Read more...

inspection of iglidur

Measuring of standard catalogue bearings

Fred Lu | August 7, 2020

iglidur® bearings are press-fit bearings for bores with a H7 standard bore. On the one hand, this press-fitting fixates the bearings in the housing and on the other, the inner diameter of the bearings is formed by that and finally creates the proper inner tolerance. If you measure the loose bearings as delivered, the inner- […]

Read more...

damage thermostat

automotive electronic thermostat bearing ——iglidur® H1

Lynna Liu (刘银) | June 28, 2020

The automotive thermostat is a valve that controls the flow of engine coolant, whose temperature can neither be too high nor too low. The thermostat can automatically adjust the amount of water entering the radiator according to the temperature of the coolant to keep it at the optimal working temperature, which is important for the […]

Read more...

乘用车BSR噪音

How do iglidur plain bearings reduce noise in automobiles (Buzz, Squeak and Rattle)?

Lynna Liu (刘银) | June 23, 2020

In this fast changing time, some technologies may be popularized soon after they are launched. For example, the heat insulation technology is only available for high-end cars a few years ago, but now it was used by almost all cars. When designing storage spaces, quality demand from design and manufacturing engineers increasingly grow. As a […]

Read more...

multifunctional furniture

Two become one: functional furniture “Frida” unites a sofa and a writing desk

Kevin Huang | June 18, 2020

Lubrication-free and maintenance-free tribo polymer bearings from igus ensure high flexibility and long life in a new piece of furniture Working and living in confined spaces is often not so easy. Therefore, the interior design student Valeria Vysozki developed a very practical solution with her piece of furniture “Frida”. Relax on the softly upholstered sofa; […]

Read more...