Plain Bearings
Figure 1. The spoiler system of the truck A well-designed spoiler system for commercial vehicles can not only increase driving safety, but also improve fuel economy and reduce freight costs. Air-guiding devices are usually installed on the top and sides of the cab of high-roof trucks or traction vehicles. If no spoiler is installed in […]
From forklifts to packaging machines: isense plain bearings provide information about their wear and warn in good time before the stoppage of plant or machinery. (Source: igus GmbH)
There are “invisible” pipelines in high-rise buildings—air conditioning ventilation system and fire safety system, which coordinate the temperature adjustment to ensure a good air environment in the building, or to reduce property losses in fire and ensure personal safety. Valves are a key component of the system. This article will introduce you to the application […]
Not since the breakthrough of additive manufacturing processes, such as laser sintering and 3D printing, has a variety of tools been available for creating polymer components and parts. Now there are no limits to the imagination. The only problem is that thanks to 3D printing, dreams of plastic are facing a nasty surprise. Often it […]
Coordinated thermal management is essential for the vehicle to be as efficient as possible. Under the optimal operating temperature, the highest efficiency and therefore the lowest consumption and the minimum emissions are achieved. The coolant plays an important role in this, as well as cooling to protect against corrosion and prevent frost. Coolant pumps, controllers […]