Category:

Plain Bearings

Polymer ball bearings in cleaning systems for photovoltaic installations

Daniel Chen | July 1, 2021

The weather is getting nicer and the sun is shining longer and more intensively. It is not only us humans who replenish energy, photovoltaic systems literally do so. These are exposed to enormous weathering effects all year round, and the surfaces reflect this especially when the sun shines…

Read more...

xiros定制滚珠轴承

Ball bearings according to specifications – an infinite number of possibilities thanks to igus®

Daniel Chen | June 24, 2021

Ball bearings cover a wide range of different shapes. Whether deep groove ball bearings, ball bearings with flange, for example, or self-aligning ball bearings: standard catalogues list these in various materials, designs and dimensions. But what about customised solutions? Customised ball bearings are no stranger to igus…

Read more...

How do the balls get into the ball bearing?

Daniel Chen | April 1, 2021

Ball bearings consist of an inner and outer ring, a cage and rolling elements. The cage is used to separate the rolling elements from each other in the form of balls. If the balls were not separated, they would run against each other and overheat. With high rotational speeds and friction of the balls, destructive effects are the result. But how do the balls get into the ball bearing now?

Read more...

Low-cost plate handling laboratory

Scott Xiong | March 23, 2021

Why use automation in the laboratory?Many small laboratories want to optimise their processes and increase their throughput rates but recoil at the frequently high costs and time-consuming integration work, when only simple combinations of devices or magazines are required…

Read more...

Plain bearing prototypes for new developments or tests

Ahren Xia | March 18, 2021

iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, round bars, or hollow rods made of various high-performance iglidur polymers & in a wide range of sizes and dimensions.

Read more...

易格斯滑动轴承

With which shafts do polymer plain bearings work best?

Ahren Xia | March 5, 2021

Many different shaft materials are used in the packaging, food and beverage industries. If a cost-effective solution is required, steel shafts are of interest. If light weight is important, aluminium shafts are used. If the application takes place in a humid environment or aggressive cleaning with chemicals, the corrosion resistance of the shaft is important. Stainless steel is a good choice here…

Read more...

金属滚珠轴承VSxiros轴承

Where metal ball bearings reach their limits: an opportunity for the polymer version?

Daniel Chen | March 4, 2021

Metal ball bearings have become indispensable in mechanical and plant engineering. However, there are sectors where conventional metal ball bearings reach their limits, such as the food industry and medical technology. There the factor of hygiene plays a major role, whereby lubricants become a no-go. This is where plastic ball bearings come into the limelight, which the Cologne-based motion plastics specialist igus manufactures with the aid of its high-performance polymers. They are absolutely lubrication-free and pose no hygiene risk…

Read more...

金属滚珠材质

What materials are used to make ball bearing balls?

Daniel Chen | February 26, 2021

The material for rolling bearing ball bearing balls varies widely and is always primarily oriented on the ring materials. This ensures that the interplay of cage, inner ring, and outer ring in the system is harmonised. This is especially important when the application involves heating or cooling the bearings. It is important that ball bearing running properties are always good. The most common ball materials are listed below with relation to the ring material…

Read more...

无润滑滑动轴承

Lubrication-free synchronisation with plain bearing technology

Ahren Xia | February 4, 2021

There are many different possibilities to synchronise several adjustments in one system. But which is the right one for me and my application? Often not easy to answer. But what if it should be simple and uncomplicated?

Read more...

跳动辊

How the weight of dancer rollers can be reduced at film deflection points

Ahren Xia | February 3, 2021

Weight is constantly what people are worried about. How can I eliminate unnecessary weight and reduce the drive forces I need? Or, simply, how can I reduce my system’s weight?

Read more...