Plain Bearings
When do I use a particular ball bearing? – Metal, plastic, ceramic.Choosing the right material for ball bearings is not always easy. A short summary, when I use a particular ball bearing…
The safety of food and drink is crucial to the well-being and health of people around the world. The cleaning and disinfection of food and beverage machines is therefore extremely important…
This is an online seminar organized by igus.inc. The speakers made a thorough study on noise, noise sources, noise reduction solvement, and related applications such as pedals, steering gear, seats and hinges. The logic is clear and the reference cases are very valuable. The duration is about 24 minutes. Welcome to click and watch!
Vending machines are becoming increasingly popular not only among farmers. It’s been a long time since they only served packaged drinks and snacks. Whoever loves to get hot pizza, fried chips or even milk from the farmer, he or she can get it from a vending machine around the corner.All this around the clock without employees..
Maintenance is a central point when operating machines. On the one hand, this ensures operational safety. On the other hand, maintenance is associated with expenditure. This expenditure is divided up as follows: The machine is at a standstill during maintenance. Depending on the machine, this is expensive. A construction machine cannot be rented. And problematic depending […]
During extrusion polymers are continuously melted and extracted through the extrusion die and brought into shape. In this way, bar stock such as filaments, profiles, plates or films emerge; the so-called extrudate…
Almost all cars are now equipped with differentials. What is its function?The differential of a car is the system that regulates how fast the tires rotate individually and helps you turn left and right. So differentials solve the cornering problem, but they come with a huge disadvantage for off-road driving. Supose that a right wheel […]
In a motion structure, a shaft and a bearing constitute an operating unit. In this sense, wear and friction values need to be evaluated from an overall perspective. To optimize lives, materials of the shaft and the bearing need to be perfectly coordinated, which is a main challenge for bearing manufacturers today. For the shaft, […]
In order for an assembly or component to be allowed for use in a modern rail vehicle in Europe, the components must be tested and evaluated according to EN45545. This is a very time-consuming, bureaucratic process. The exposed surface, the weight of the component, and many other points must be considered for selection. So where […]
When refering to modified vehicles, we are now easily thinking about a foldable steps of SUV,especially those with high chassis. In order to help passengers to easily get on and off, installing a set of steps is almost a must. There are 2 types of step for your option:fixed or foldable. Nowadays more and more […]