second
required for theme
Vending machines are becoming increasingly popular not only among farmers. It’s been a long time since they only served packaged drinks and snacks. Whoever loves to get hot pizza, fried chips or even milk from the farmer, he or she can get it from a vending machine around the corner.All this around the clock without employees..
Especially in times of crisis, creative and above all fast solutions are essential. And when it comes to speed and creativity, the 3D printing community is quick to respond. This was also the case this time when Prusa Research…
The proportion of electronic and electromechanical components in vehicles has been growing continuously for years. The increased comfort and the growing safety requirements promote this development.
Lean automation: igus Robot Control with 21 digital inputs and outputs Behind Low Cost Automation is cost savings and great productivity provided by modularity, user-friendliness and reliability. To make robot programming and control even easier, igus has added the igus Robot Control to its Low Cost Automation range. What is special here is that up to 21 […]
Large bearing diameters tailor-made at an off-the-shelf price! The largest selection of different dimensions is offered by “the generalist” iglidur G. The smallest bearing has an inner diameter of 3mm (smaller inner diameters are available for other iglidur materials). The largest inner diameter of an igus catalogue part is 195mm. Part No.: GFM-195205240-65 (Outer diameter 205mm, flange […]
In a motion structure, a shaft and a bearing constitute an operating unit. In this sense, wear and friction values need to be evaluated from an overall perspective. To optimize lives, materials of the shaft and the bearing need to be perfectly coordinated, which is a main challenge for bearing manufacturers today. For the shaft, […]
Widespread in the animal kingdom, for people an option. The skeleton on the outside of arthropods provides stability in the same way as the endoskeletons of mammals. Why not combine the advantages of the two systems with each other? An endoskeleton (inside the body) is strong but, having numerous joints, is nevertheless very flexible. It […]
When refering to modified vehicles, we are now easily thinking about a foldable steps of SUV,especially those with high chassis. In order to help passengers to easily get on and off, installing a set of steps is almost a must. There are 2 types of step for your option:fixed or foldable. Nowadays more and more […]
Grease or lubricating oil is essential for installing metal ball bearings. With xiros polymer ball bearings you can enjoy 100% lubrication-free ball bearings made of plastic. No grease No oil No residues on hands or machines!
We get asked this question quite often, the brief explanation by sellers sometimes cannot be accepted by or not satisfy customers! Of course, we do fully understand the customers’ complaints about this situation. For example, the customer is designing a device, the linear bearing system involved is of great importance for them, which may also […]