Keyword:

food industry

食品行业

Plain bearing prototypes for new developments or tests

Ahren Xia | March 18, 2021

iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, round bars, or hollow rods made of various high-performance iglidur polymers & in a wide range of sizes and dimensions.

Read more...

易格斯滑动轴承

With which shafts do polymer plain bearings work best?

Ahren Xia | March 5, 2021

Many different shaft materials are used in the packaging, food and beverage industries. If a cost-effective solution is required, steel shafts are of interest. If light weight is important, aluminium shafts are used. If the application takes place in a humid environment or aggressive cleaning with chemicals, the corrosion resistance of the shaft is important. Stainless steel is a good choice here…

Read more...

球轴承

Spherical bearings for weigher flaps

Ahren Xia | January 25, 2021

igubal spherical bearings are self-aligning bearing elements manufactured completely from polymer and are therefore very lightweight. They are perfect for use in weighing systems…

Read more...

小空间安装的直线导向系统

Linear guides for limited installation space

Ahren Xia | December 29, 2020

igus has many different linear guides in its product range. For example, drylin W offers a large modular system. drylin N is the first choice for extremely low-profile installation heights. drylin T is identical in construction to the usual recirculating ball bearing guides. A representative of the shaft guides is drylin R. Since some machine […]

Read more...

食品机械

Severe contamination by salt or sugar … what must be observed?

Ahren Xia | December 23, 2020

Wherever food or beverages are processed, filled or packed, contamination can occur. If it is salt or sugar, it is important to take a close look at the abrasive (rubbing/grinding) wear. In this way it can be determined what influence this has on the plain bearing or linear guide…

Read more...

直线技术

Ready-to-install system solutions for format adjustments

Ahren Xia | December 22, 2020

To maximise flexibility, machines and equipment in the packaging, food and beverage industries must be capable of implementing precise format adjustments. This equipment might be filling or labelling machines for bottles or cans, but can also be entry lanes in material handling…

Read more...

食品级运动塑料部件

Are there detectable plastics with food approval for moving applications?

Ahren Xia | December 7, 2020

We have often dealt with this problem. Simple plain bearings are used in most applications. As these are usually seated with a positive fit and fixed in a housing hole, it is almost impossible for them to fall out or break…

Read more...

化学抗性

Chemical resistance to Ecolab cleaners

Ahren Xia | December 1, 2020

The safety of food and drink is crucial to the well-being and health of people around the world. The cleaning and disinfection of food and beverage machines is therefore extremely important…

Read more...

食品认证

Certifications for the food and beverage industry

Ahren Xia | September 18, 2020

Since food and beverages are sensitive products, production and processing must also be precisely tailored to them. This applies in particular to direct food contact.For this reason, there are igus materials that have been specifically developed for the requirements of the food and beverage industry.

Read more...

miromatic公司专注于生产水果酸奶搅拌和桶装食品灌装设备,是这一领域的欧洲企业领导者。

Hygienic design with plastic plain bearings

Ahren Xia | September 16, 2020

Manufacturer of filling systems, miromatic, uses the igus modular construction kit Machines from miromatic fill containers with foodstuffs such as yoghurt fully automatically. The requirements regarding the hygiene and availability of the machines in such cases are high. The igus plain bearings made of high-performance plastics with incorporated lubricant prove their worth under these conditions.In […]

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18