Keyword:

Beverage industry

饮料行业

Plain bearing prototypes for new developments or tests

Ahren Xia | March 18, 2021

iglidur polymer bar stock allows such components to be manufactured easily … with no minimum order quantity. It is available as plates, round bars, or hollow rods made of various high-performance iglidur polymers & in a wide range of sizes and dimensions.

Read more...

易格斯滑动轴承

With which shafts do polymer plain bearings work best?

Ahren Xia | March 5, 2021

Many different shaft materials are used in the packaging, food and beverage industries. If a cost-effective solution is required, steel shafts are of interest. If light weight is important, aluminium shafts are used. If the application takes place in a humid environment or aggressive cleaning with chemicals, the corrosion resistance of the shaft is important. Stainless steel is a good choice here…

Read more...

无润滑滑动轴承

Lubrication-free synchronisation with plain bearing technology

Ahren Xia | February 4, 2021

There are many different possibilities to synchronise several adjustments in one system. But which is the right one for me and my application? Often not easy to answer. But what if it should be simple and uncomplicated?

Read more...

耐磨带包装

Can products in entry lanes be protected from damage?

Ahren Xia | January 28, 2021

The concern is often optimisation of component or system service life. In the packaging and beverage industries, machines operate at especially high frequencies, and component service life plays an important role. But it can be just as important to extend the product service life or life cycle. ..

Read more...

小空间安装的直线导向系统

Linear guides for limited installation space

Ahren Xia | December 29, 2020

igus has many different linear guides in its product range. For example, drylin W offers a large modular system. drylin N is the first choice for extremely low-profile installation heights. drylin T is identical in construction to the usual recirculating ball bearing guides. A representative of the shaft guides is drylin R. Since some machine […]

Read more...

直线技术

Ready-to-install system solutions for format adjustments

Ahren Xia | December 22, 2020

To maximise flexibility, machines and equipment in the packaging, food and beverage industries must be capable of implementing precise format adjustments. This equipment might be filling or labelling machines for bottles or cans, but can also be entry lanes in material handling…

Read more...

化学抗性

Chemical resistance to Ecolab cleaners

Ahren Xia | December 1, 2020

The safety of food and drink is crucial to the well-being and health of people around the world. The cleaning and disinfection of food and beverage machines is therefore extremely important…

Read more...

食品认证

Certifications for the food and beverage industry

Ahren Xia | September 18, 2020

Since food and beverages are sensitive products, production and processing must also be precisely tailored to them. This applies in particular to direct food contact.For this reason, there are igus materials that have been specifically developed for the requirements of the food and beverage industry.

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18