Keyword:

xiros

滚珠轴承

ticket machine

Why your ticket machine ball bearings should be from igus®

Daniel Chen | September 24, 2021

Ball bearings in ticket machines where requirements for installed components are stringent. igus polymer ball bearings are expanding their advantage over metal ball bearings in this segment. They are not only maintenance-free and lubrication-free – they also ensure that the application environment is free of contamination. Searching for contamination…

Read more...

滚珠轴承的替换

Ball bearing alternative made of polymer: igus® convinces

Daniel Chen | September 17, 2021

Many plant operators know the problem: when installing metal ball bearings, lubrication is essential. This procedure has to be repeated at regular maintenance intervals and that not only swallows up money, but also a lot of time. As a ball bearing alternative, xiros is particularly suitable…

Read more...

易格斯自润滑免维护轴承

When should I change my ball bearing?

Daniel Chen | August 13, 2021

Change the ball bearing? This should be done, when …

the bearing clearance caused by wear has reached an unacceptable level, for example, when the shaft “sags”.
the cage is worn and in danger of falling out.

Read more...

Polymer ball bearings in cleaning systems for photovoltaic installations

Daniel Chen | July 1, 2021

The weather is getting nicer and the sun is shining longer and more intensively. It is not only us humans who replenish energy, photovoltaic systems literally do so. These are exposed to enormous weathering effects all year round, and the surfaces reflect this especially when the sun shines…

Read more...

xiros

Time for a dive into cool waters – xiros® in pools cleaner ensures the necessary cleanliness in the pool

Daniel Chen | December 30, 2020

The holiday is shifting into your own four walls. If the temperatures exceed the limit of 30°C, the only thing that helps is to jump into the cool water. Butpool lovers know the problems with a pool in the garden. The autumn and winter months do not go by without leaving their mark. Dirt, leaves and moss accumulate and cleaning turns out to be an arduous task. I need a pool cleaner…

Read more...

How igus products increase the service life of your extrusion line and avoid production downtime

John Ji | November 10, 2020

During extrusion polymers are continuously melted and extracted through the extrusion die and brought into shape. In this way, bar stock such as filaments, profiles, plates or films emerge; the so-called extrudate…

Read more...

无润滑球轴承

Why lubrication-free is a better option for your ball bearing

Daniel Chen | September 18, 2020

Grease or lubricating oil is essential for installing metal ball bearings. With xiros polymer ball bearings you can enjoy 100% lubrication-free ball bearings made of plastic. No grease No oil No residues on hands or machines!

Read more...

A / C旋钮

Vehicle interior – 3 examples of polymer ball bearings in control elements

Lynna Liu (刘银) | September 16, 2020

The modern car interior has many different knobs, dials and switches. Whether it is the adjustment of the window, air conditioning or sound level – we are increasingly resorting to the cleverly placed rotary adjusters in the interior. All these controls are directly related to the quality perception of the vehicle and can influence a […]

Read more...

主动进气格栅

Active Air Intake Grille

Lynna Liu (刘银) | August 31, 2020

The Xiros self-lubricating plastic ball bearing is adopted for the shutter mechanism of the active air intake grille, which could perfectly meet the requirements of the customers: it features minimum friction coefficient, dirt resistance, resistance to high temperature and low temperature and light weight. For vertical shutter, we also provide iglidur J sliding bearing for […]

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18