Keyword:

Lead screw system

丝杠系统

啤酒升降机

Lead screw technology in the DIY beer lift

Kevin Huang | September 25, 2020

Beer lift light built with maintenance-free lead screw technology. High temperatures in summer, the need for a cool drink but no desire to constantly run to the fridge? The self-built beer lift provides a solution. Up to 21 beverage bottles can be cooled in the stylish beer lift. Completely without electricity and as a highlight […]

Read more...

重载螺母JGRM

GJRM——Heavy-duty thread

Kevin Huang | September 22, 2020

Can the heavy load be combined with threads? What are the advantages of threads in heavy-duty applications? When threads are used in heavy-duty applications, they must meet many requirements. One of the most important aspects for heavy loads is the stability of the threads under high axial and radial loads. But does this also work […]

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18