Current carrying capacity of cables

Jen Chen | October 25, 2021

maximum current carrying capacity values listed for chainflex cables, refer not only to the electrical limit values but also to the special mechanical load in the energy chain. These values therefore offer a higher degree of safety than usual standard values.

Read more...

How a new path began at Ethernet

Jen Chen | September 15, 2021

At igus, we rely on our partner HARTING for cable harnessing. There were different reasons for this association. In addition to the quality of the products, this also includes delivery reliability and ease of assembly.

Read more...

Cables in industrial doors

Jen Chen | September 15, 2021

Choose the right cable for your industrial door——Choosing the right cables was not quite as easy as it seems at first glance. Sometimes it takes more than just a look in the catalogue. Here, not only the external influences, such as the ambient temperature, must be taken into account, but also application-based specifications.

Read more...

Bus cables for long travels and the alternatives

Jen Chen | September 15, 2021

With a fibre optic cable you can also transmit a signal over long distances. This is due to the significantly lower attenuation values compared to a copper cable.

Read more...

Why copper? Copper as a conductor material?

Jen Chen | August 16, 2021

Haven’t you ever wondered why cables are mostly made of copper and why there are such exotics where precious metals like gold and silver are used? Copper as a conductor material has its reasons. That’s what we’re talking about today.

Read more...

Flame-retardant TPE and halogen-free TPE

Jen Chen | August 16, 2021

There are countless materials in the world. But very few come into question for the cable industry. The most frequently used jacket materials in cable technology are PVC and PUR. But, in addition to these two outer jacket materials, we at igus use TPE (thermoplastic elastomers). However, not all TPEs are created equal. That is why our article today will deal with the different TPE mixtures – flame-retardant TPE and halogen-free TPE.

Read more...

Cables for extreme heat

Jen Chen | August 16, 2021

utdoors often have to withstand seasonal temperature fluctuations. Due to the extreme temperatures in recent years, we therefore also have to consider this issue when choosing the right cable. Therefore, today’s topic is cables in extreme heat and the effects of high ambient temperatures on energy chain cables.

Read more...

PM5420_E4Q_German-Design-Award

Harnessing the secrets of nature: the E4Q energy chain from igus wins the German Design Award

Jen Chen | December 15, 2020

The latest energy chain generation design saves weight, increases strength and reduces assembly time by 40 per cent

Read more...

PM4520_igubal-ESQM

Suitable for the desert! igubal pillow block bearings without lubrication align solar panels

Jen Chen | December 15, 2020

Extended igus solar pillow block bearing series for square profiles, impresses in laboratory tests with a service life of over 72 years

Read more...

PM0220-Cat-HTR-investor

When plastic becomes oil again: igus invests in chemical recycling pioneer

Jen Chen | October 23, 2020

Cat-HTR technology developed by a German scientist regains resources from plastic waste in 20 minutes

Read more...