Ready for direct connection: igus hybrid cable for new motor generation

Jen Chen | June 30, 2020

The new cost-effective hybrid cable suitable for Bosch Rexroth motors ensures a reliable supply of energy and data during motion. (Source: igus GmbH)

Read more...

damage thermostat

automotive electronic thermostat bearing ——iglidur® H1

Lynna Liu (刘银) | June 28, 2020

The automotive thermostat is a valve that controls the flow of engine coolant, whose temperature can neither be too high nor too low. The thermostat can automatically adjust the amount of water entering the radiator according to the temperature of the coolant to keep it at the optimal working temperature, which is important for the […]

Read more...

Turbolader 涡轮增压塑料连杆

Coupling joints made of polymer – optimised materials for the automotive industry

Lynna Liu (刘银) | June 24, 2020

The coupling joint, also referred to as double joint, describes a strut with connection possibilities on both sides. Here, ball and socket joints, screw threads or sleeves can be inserted, which connect the coupling joint with the corresponding vehicle components. Usually, coupling joints are made of steel or aluminium. But for years, polymer coupling joints […]

Read more...

乘用车BSR噪音

How do iglidur plain bearings reduce noise in automobiles (Buzz, Squeak and Rattle)?

Lynna Liu (刘银) | June 23, 2020

In this fast changing time, some technologies may be popularized soon after they are launched. For example, the heat insulation technology is only available for high-end cars a few years ago, but now it was used by almost all cars. When designing storage spaces, quality demand from design and manufacturing engineers increasingly grow. As a […]

Read more...

multifunctional furniture

Two become one: functional furniture “Frida” unites a sofa and a writing desk

Kevin Huang | June 18, 2020

Lubrication-free and maintenance-free tribo polymer bearings from igus ensure high flexibility and long life in a new piece of furniture Working and living in confined spaces is often not so easy. Therefore, the interior design student Valeria Vysozki developed a very practical solution with her piece of furniture “Frida”. Relax on the softly upholstered sofa; […]

Read more...