“We look forward to the next complaint”

Jen Chen | September 1, 2022

When I first heard this statement over 15 years ago, I thought, “We can’t be serious.” A complaint is a bad thing, it costs money, damages reputation, causes discord and involves a lot of work. Today, I stand rock solid behind that very statement. But why?

Read more...

What is a corkscrew in a cable and how can it be avoided?

Jen Chen | August 31, 2022

Those who deal with cables or use cables in their applications are often familiar with the so-called corkscrew. Today we would like to explain what a corkscrew is, how it develops and of course how it can be avoided.

Read more...

What is a BUS?

Jen Chen | August 31, 2022

When people think of the term “bus”, most of them immediately think of a school bus or public transport bus. But in our case this has nothing to do with the vehicle. BUS is an abbreviation that stands for “Binary Unit System”.

Read more...

Works on more than 1,000 metres: igus develops the world’s first driven e-chain system for long travels

Jen Chen | August 9, 2022

drive-chain impresses with maximum dynamics and long service life, while saving up to six tons of weight Almost no limits on long travels, high dynamics, long running times – these are the characteristics that distinguish the innovative igus drive-chain. The world’s first energy chain with its own drive ensures significantly longer running times on extremely long […]

Read more...

What is CC-Link?

Jen Chen | June 16, 2022

CC-Link is a worldwide used bus system, which is offered as a conventional fieldbus system, but also as Ethernet based. There are many applications for these cables. These can be either static or moving in energy chains.

Read more...

Underwater cables

Jen Chen | June 10, 2022

We at igus have specialised in cables for moving applications. Our chainflex cables are therefore only suitable for applications with low or periodic water influence and not for continuous use deep under water.
The reason for this, is that we must ensure the materials’ abrasion resistance, and we cannot do this with rubber-like outer jackets.

Read more...

How igus® responds innovatively to challenges of modern manufacturing

Jen Chen | June 9, 2022

A brief look at the igus history shows: new challenges also always hold opportunities for new products and markets.
If the market does not offer adequate solutions, it is possible to create new production and test standards with good ideas, precision and a lot of care.

Read more...

Can fibre optic cable be the solution for small bend radii?

Jen Chen | May 13, 2022

Industry 4.0 has now found its way into very many applications. Data is collected at a wide variety of points and must be conveyed to the control system. Used here among other things are our chainflex cables. But when is fibre optic cable the right solution? And can fibre optic cable be used with small bend radii? We would like to take a closer look at that today.

Read more...

Where are cables used?
chainflex cables used at great heights

Jen Chen | May 13, 2022

Regardless of the application area you are dealing with, igus® has made it its business to find a cable that meets all requirements. Benefit from our variety of cables. From low-cost solutions with PVC outer jacket to high-end TPE cables. Everything in line with our motto: Cost down, life up!

Read more...

Why does igus offer so many different cable types of the same kind?

Jen Chen | May 13, 2022

We have introduced the chainflex Class. This should help to select the right cable based on the criteria of stress, travel, oil resistance and torsion. The higher the number, the better the cable.

Read more...