After the successful completion of the audit we also received our own UL Verified logo. The UL test mark with the number B129699 is an individual recognition feature. It allows the purchaser to look up more information online about the specific chainflex product promise verified by UL. This makes it easy for the customer to decide on chainflex.
The new 2020 chainflex catalogue is ready!
“We replace the cables on the machine every six weeks. Well, that’s normal!” We hear sentences like these time and again in our industry. Very few users are aware that this condition is not normal. Choosing the right cable makes the difference. In this article I would like to explain why flexible cables are not […]
maximum current carrying capacity values listed for chainflex cables, refer not only to the electrical limit values but also to the special mechanical load in the energy chain. These values therefore offer a higher degree of safety than usual standard values.
Ball bearings in ticket machines where requirements for installed components are stringent. igus polymer ball bearings are expanding their advantage over metal ball bearings in this segment. They are not only maintenance-free and lubrication-free – they also ensure that the application environment is free of contamination. Searching for contamination…