塑料轴承材料

What is iglidur? And what does it do better than POM?

John Ji | August 26, 2020

Just recently I stumbled on this blog post, which promised to finally put an end to the mystery that seems to be iglidur®. What is iglidur? And why are customers willing to spend no less than a fortune on bearings made from this material? To make this clear right away: I have no intention to […]

Read more...

vector 2020

Automatic lathe with six spindles wins gold vector award

Jen Chen | August 17, 2020

Gildemeister Italiana S.p.A. wins first prize for a unique energy chain system

Read more...

Advantages of polymer bearings in the bicycle

John Ji | August 10, 2020

In the bicycle industry, innovative solutions are not only focused on design, but also on the choice of materials. For example, for the frame there are many solutions made of aluminium or glass fibre reinforced material. Component manufacturers are also working flat out on the use of alternative materials. Be it saddle post, suspension, pedals […]

Read more...

Angular compensation

Angular compensation in rail vehicle construction

Kevin Huang | August 10, 2020

Whether in a welded construction of a road/rail vehicle, or in the interior of a double-decker train; you have to work with tolerances everywhere and be able to compensate for them. Especially when linear, pivoting or rotary movements should continue to function without problems. There are often linear guides used in railway construction vehicles or […]

Read more...

Application Trend of Motion Plastics in Seat Systems

Lynna Liu (刘银) | August 7, 2020

On June 27, 2020, Shanghai officially announced the launch of Didi’s self-driving service online, which signify that driverless technology and applications have basically matured. Without a driver, or the driver adjusts to automatic driving mode, the internal space of a car can be transformed into entertainment room,or games, rest , meeting room. Passengers can adjust […]

Read more...