Keyword:

Xiors

Xiros滚珠轴承

汽车内饰

Why are polymer ball bearings so interesting for vehicle interiors?

Ethen Liang | August 19, 2021

Developing the interiors of cars is a big challenge for designers and engineers. Within just a few seconds, it creates a first gut feeling. Even before we sit down on the car seat, we reach for the steering wheel. Immediately afterwards, we examine the arm rest and feel the buttons for adjusting the windows…

Read more...

易格斯自润滑免维护轴承

When should I change my ball bearing?

Daniel Chen | August 13, 2021

Change the ball bearing? This should be done, when …

the bearing clearance caused by wear has reached an unacceptable level, for example, when the shaft “sags”.
the cage is worn and in danger of falling out.

Read more...

xiros定制滚珠轴承

Ball bearings according to specifications – an infinite number of possibilities thanks to igus®

Daniel Chen | June 24, 2021

Ball bearings cover a wide range of different shapes. Whether deep groove ball bearings, ball bearings with flange, for example, or self-aligning ball bearings: standard catalogues list these in various materials, designs and dimensions. But what about customised solutions? Customised ball bearings are no stranger to igus…

Read more...

金属滚珠轴承VSxiros轴承

Where metal ball bearings reach their limits: an opportunity for the polymer version?

Daniel Chen | March 4, 2021

Metal ball bearings have become indispensable in mechanical and plant engineering. However, there are sectors where conventional metal ball bearings reach their limits, such as the food industry and medical technology. There the factor of hygiene plays a major role, whereby lubricants become a no-go. This is where plastic ball bearings come into the limelight, which the Cologne-based motion plastics specialist igus manufactures with the aid of its high-performance polymers. They are absolutely lubrication-free and pose no hygiene risk…

Read more...

金属滚珠材质

What materials are used to make ball bearing balls?

Daniel Chen | February 26, 2021

The material for rolling bearing ball bearing balls varies widely and is always primarily oriented on the ring materials. This ensures that the interplay of cage, inner ring, and outer ring in the system is harmonised. This is especially important when the application involves heating or cooling the bearings. It is important that ball bearing running properties are always good. The most common ball materials are listed below with relation to the ring material…

Read more...

跳动辊

How the weight of dancer rollers can be reduced at film deflection points

Ahren Xia | February 3, 2021

Weight is constantly what people are worried about. How can I eliminate unnecessary weight and reduce the drive forces I need? Or, simply, how can I reduce my system’s weight?

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18