Notice: Function _load_textdomain_just_in_time was called incorrectly. Translation loading for the business-units-for-igus domain was triggered too early. This is usually an indicator for some code in the plugin or theme running too early. Translations should be loaded at the init action or later. Please see Debugging in WordPress for more information. (This message was added in version 6.7.0.) in /var/www/html/wp-includes/functions.php on line 6121 Warning: Cannot modify header information - headers already sent by (output started at /var/www/html/wp-includes/functions.php:6121) in /var/www/html/wp-content/themes/business-units-for-igus/functions.php on line 386 UL certificate – 易格斯新闻技术资讯

Keyword:

UL certificate

UL认证

What is FastConnect?

Jen Chen | February 28, 2022

FastConnect delivers what it promises. It works quickly and without complications. Because you only need one tool for this. With this technology you can achieve a time saving of up to 46%. The machine can restart quickly and you do not lose any time. And above all, no money.

Read more...

Flame-retardant TPE and halogen-free TPE

Jen Chen | August 16, 2021

There are countless materials in the world. But very few come into question for the cable industry. The most frequently used jacket materials in cable technology are PVC and PUR. But, in addition to these two outer jacket materials, we at igus use TPE (thermoplastic elastomers). However, not all TPEs are created equal. That is why our article today will deal with the different TPE mixtures – flame-retardant TPE and halogen-free TPE.

Read more...