Keyword:

Sealing

密封

The right shaft for tough outdoor use – if the plain bearing is outdoors.

Yvan Cao | October 28, 2020

Everyone knows that the agricultural and construction machinery sector require lots of care. Dirt, moisture, corrosion, the complete package. Whether a combine harvester, tractor, concrete mixer, plough or mobile crane – here everything is in the same boat. Metallic plain bearings are always lubricated – at least they should be if they are to function. […]

Read more...

seal iglidur

Seal for plain bearings: What are the approaches available?

Sebastian | April 24, 2020

Too much dirt in the bearing? Basically, many plain bearings – depending on the type – are much less sensitive to dirtthan rolling bearings. But as it often happens, if it’s too much, it’s too much.At the latest when the entire bearing clearance is filled with dirt, no one is wonderingabout problems. Especially with abrasive […]

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18