Keyword:

Deep groove ball bearing

滚珠轴承的替换

Ball bearing alternative made of polymer: igus® convinces

Daniel Chen | September 17, 2021

Many plant operators know the problem: when installing metal ball bearings, lubrication is essential. This procedure has to be repeated at regular maintenance intervals and that not only swallows up money, but also a lot of time. As a ball bearing alternative, xiros is particularly suitable…

Read more...

易格斯自润滑免维护轴承

When should I change my ball bearing?

Daniel Chen | August 13, 2021

Change the ball bearing? This should be done, when …

the bearing clearance caused by wear has reached an unacceptable level, for example, when the shaft “sags”.
the cage is worn and in danger of falling out.

Read more...

How do the balls get into the ball bearing?

Daniel Chen | April 1, 2021

Ball bearings consist of an inner and outer ring, a cage and rolling elements. The cage is used to separate the rolling elements from each other in the form of balls. If the balls were not separated, they would run against each other and overheat. With high rotational speeds and friction of the balls, destructive effects are the result. But how do the balls get into the ball bearing now?

Read more...

金属滚珠材质

What materials are used to make ball bearing balls?

Daniel Chen | February 26, 2021

The material for rolling bearing ball bearing balls varies widely and is always primarily oriented on the ring materials. This ensures that the interplay of cage, inner ring, and outer ring in the system is harmonised. This is especially important when the application involves heating or cooling the bearings. It is important that ball bearing running properties are always good. The most common ball materials are listed below with relation to the ring material…

Read more...

Where are ball bearings used? And what kinds of ball bearings are there?

Daniel Chen | December 10, 2020

Ball bearings have become indispensable in mechanical engineering. There are various ball bearing designs for which mass and technical composition of the components depend on the specifications of the industrial application. The following list shows the most frequently used ball bearings and where they are used…

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18