Keyword:

chainflex

电缆

What is a corkscrew in a cable and how can it be avoided?

Jen Chen | August 31, 2022

Those who deal with cables or use cables in their applications are often familiar with the so-called corkscrew. Today we would like to explain what a corkscrew is, how it develops and of course how it can be avoided.

Read more...

What is a BUS?

Jen Chen | August 31, 2022

When people think of the term “bus”, most of them immediately think of a school bus or public transport bus. But in our case this has nothing to do with the vehicle. BUS is an abbreviation that stands for “Binary Unit System”.

Read more...

At last! The new 2020 chainflex catalogue is ready!

Jen Chen | October 25, 2021

The new 2020 chainflex catalogue is ready!

Read more...

Why flexible cables are not a wear-resistant part

Jen Chen | October 25, 2021

“We replace the cables on the machine every six weeks. Well, that’s normal!” We hear sentences like these time and again in our industry. Very few users are aware that this condition is not normal. Choosing the right cable makes the difference. In this article I would like to explain why flexible cables are not […]

Read more...

CFROBOT8.PLUS: chainflex Ethernet cable

3D Ethernet cable from igus enables fast robot communication

Marck Liu (刘奕驰) | May 19, 2020

Tested chainflex cable for torsion angles up to 360 degrees safely transmits data to 6-axis robots In large-scale manufacturing industrial robots are everywhere. They provide a fast automation of processes and thereby ensure cost-efficiency in companies. igus has now developed a new long-lasting Ethernet cable, the CFROBOT8.PLUS, to ensure that robot communication between the axes, […]

Read more...

new highly flexible chainflex cables CFBUS.045 and CFBUS.049

Highly flexible Ethernet cables with 600 Volt UL certificate for Industry 4.0

Marck Liu (刘奕驰) | May 19, 2020

New CAT5e and CAT6 cables for use in e-chain with increased service life and approval for the American market CAT5e or CAT6 cables are indispensable for the implementation of Industry 4.0 in automation. igus has now further developed two highly flexible Ethernet cables, CFBUS.045 and CFBUS.049, specifically for use in the energy chain. The new […]

Read more...

New chainflex Ethernet cables with CC-Link IE

Highly flexible Ethernet cables for e-chains with CC-Link IE Field certificate

Marck Liu (刘奕驰) | May 19, 2020

New chainflex CAT5e and CAT6 cables with predictable and guaranteed service life and certification for CC-Link IE protocolsCAT5e or CAT6 cables are indispensable for the implementation of Industry 4.0 in automation. igus has now developed two highly flexible Ethernet cables, CFBUS.045 and CFBUS.049, for use in energy chains. The new cables have now been tested […]

Read more...

电缆的igus新型绝缘材料

Safe protection for the next generation of motors with new igus material

Marck Liu (刘奕驰) | May 18, 2020

Optimised insulation of chainflex VFD motor and servo cables for energy chain use, thanks to new high-performance polymer The trend for variable frequency drives (VFDs) is moving towards more compact drives with the same or higher power and extremely high switching accuracies of the frequency converters. As a result, when selecting the cable the user […]

Read more...

Technical revolution in automatic turning

Sebastian | April 24, 2020

igus develops energy supply solution for rotational and linear motion for DMG MORI After only two years of development time, DMG MORI ushers in a new era of automatic turning machines with multiple spindles. The current MULTISPRINT series represents a technological revolution in automatic turning. The efficient turning machine itself and also the fast, precise […]

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18