Keyword:

Bearing material

轴承材料

金属滚珠材质

What materials are used to make ball bearing balls?

Daniel Chen | February 26, 2021

The material for rolling bearing ball bearing balls varies widely and is always primarily oriented on the ring materials. This ensures that the interplay of cage, inner ring, and outer ring in the system is harmonised. This is especially important when the application involves heating or cooling the bearings. It is important that ball bearing running properties are always good. The most common ball materials are listed below with relation to the ring material…

Read more...

塑料轴承材料

What is iglidur? And what does it do better than POM?

John Ji | August 26, 2020

Just recently I stumbled on this blog post, which promised to finally put an end to the mystery that seems to be iglidur®. What is iglidur? And why are customers willing to spend no less than a fortune on bearings made from this material? To make this clear right away: I have no intention to […]

Read more...

high temperature resistance

Why can plastic plain bearings be used in the engine compartment?

Lynna Liu (刘银) | May 21, 2020

Plastic and high temperatures? Yes, even as a connection to actuators of turbochargers or in EGR valves, iglidur® high-temperature materials are represented millions of times as plain bearings or coupling rods. With permanent application temperatures of up to 250 ° C and briefly 300 ° C, plastic plain bearings are used in almost all engine […]

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18