Keyword:

Anti-rust

防锈

Under Heavy Load Application Conditions–Study on Maximum Service Lives of Shaft and Sliding Bearing

Yvan Cao | September 30, 2020

In a motion structure, a shaft and a bearing constitute an operating unit. In this sense, wear and friction values need to be evaluated from an overall perspective. To optimize lives, materials of the shaft and the bearing need to be perfectly coordinated, which is a main challenge for bearing manufacturers today. For the shaft, […]

Read more...

Deprecated: str_replace(): Passing null to parameter #3 ($subject) of type array|string is deprecated in /var/www/html/wp-content/themes/business-units-for-igus/wp_bootstrap_pagination.php on line 18