Extended igus solar pillow block bearing series for square profiles, impresses in laboratory tests with a service life of over 72 years
When an eagle grasps prey, it adapts its grip to the respective size in a lightning fast move. The packaging industry can only dream of this flexibility. Their metal grippers, which for example put the lid on cream jars, are usually limited to a single format…
Ball bearings have become indispensable in mechanical engineering. There are various ball bearing designs for which mass and technical composition of the components depend on the specifications of the industrial application. The following list shows the most frequently used ball bearings and where they are used…
We have often dealt with this problem. Simple plain bearings are used in most applications. As these are usually seated with a positive fit and fixed in a housing hole, it is almost impossible for them to fall out or break…
When do I use a particular ball bearing? – Metal, plastic, ceramic.Choosing the right material for ball bearings is not always easy. A short summary, when I use a particular ball bearing…