CFROBOT8.PLUS: chainflex Ethernet cable

3D Ethernet cable from igus enables fast robot communication

Marck Liu (刘奕驰) | May 19, 2020

Tested chainflex cable for torsion angles up to 360 degrees safely transmits data to 6-axis robots In large-scale manufacturing industrial robots are everywhere. They provide a fast automation of processes and thereby ensure cost-efficiency in companies. igus has now developed a new long-lasting Ethernet cable, the CFROBOT8.PLUS, to ensure that robot communication between the axes, […]

Read more...

new highly flexible chainflex cables CFBUS.045 and CFBUS.049

Highly flexible Ethernet cables with 600 Volt UL certificate for Industry 4.0

Marck Liu (刘奕驰) | May 19, 2020

New CAT5e and CAT6 cables for use in e-chain with increased service life and approval for the American market CAT5e or CAT6 cables are indispensable for the implementation of Industry 4.0 in automation. igus has now further developed two highly flexible Ethernet cables, CFBUS.045 and CFBUS.049, specifically for use in the energy chain. The new […]

Read more...

New chainflex Ethernet cables with CC-Link IE

Highly flexible Ethernet cables for e-chains with CC-Link IE Field certificate

Marck Liu (刘奕驰) | May 19, 2020

New chainflex CAT5e and CAT6 cables with predictable and guaranteed service life and certification for CC-Link IE protocolsCAT5e or CAT6 cables are indispensable for the implementation of Industry 4.0 in automation. igus has now developed two highly flexible Ethernet cables, CFBUS.045 and CFBUS.049, for use in energy chains. The new cables have now been tested […]

Read more...

电缆的igus新型绝缘材料

Safe protection for the next generation of motors with new igus material

Marck Liu (刘奕驰) | May 18, 2020

Optimised insulation of chainflex VFD motor and servo cables for energy chain use, thanks to new high-performance polymer The trend for variable frequency drives (VFDs) is moving towards more compact drives with the same or higher power and extremely high switching accuracies of the frequency converters. As a result, when selecting the cable the user […]

Read more...

From prototype to volume production: this is how you choose the right method

Sebastian | May 9, 2020

Not since the breakthrough of additive manufacturing processes, such as laser sintering and 3D printing, has a variety of tools been available for creating polymer components and parts. Now there are no limits to the imagination. The only problem is that thanks to 3D printing, dreams of plastic are facing a nasty surprise. Often it […]

Read more...